WinStudio

IsCurrentObjectPropertyModified Method

Applies To

IWSIDOCollection interface

Definition

Returns a Boolean value indicating whether the current object property in a specified IDO collection has been modified.

Syntax

object.IsCurrentObjectPropertyModified( string )

  Part

  Description

object Required. The name of a valid IDO collection object.
string Required. The name of the object property.

Remarks

A return value of:

If the specified IDO collection has focus, use this method. If the specified IDO collection might not have focus, use the IsObjectPropertyModified method.

Example

Sub Main()
    ReturnValue = "0"
    
    If (ThisForm.PrimaryIDOCollection.IsCurrentObjectPropertyModified(GetParameter(0)) = True And
        ThisForm.PrimaryIDOCollection.GetCurrentObjectProperty(GetParameter(0)) = "3" )
        ReturnValue = "1"
    End If
End Sub