WinStudio
IWSFormComponent interface, List component type objects
Returns a Boolean value indicating whether an entry in a list box (List type component) is the selected entry.
object.IsListBoxEntrySelected( integer )
Part |
Description |
| object | Required. A reference to a List component type object. |
| integer | Required. The zero-based index number of the list entry. |
A return value of:
NOTE: This method does not work with other list source components, such as drop-down lists, combo boxes, or grid columns.
Sub Main()
If ThisForm.Components("list1").IsListBoxEntrySelected(3) Then
Application.ShowMessage("That's the one. Good job!")
Else
Application.ShowMessage("Wrong selection! Try again.")
End If
End Sub