WinStudio
IWSIDOCollection interface
Returns a Boolean value indicating whether the object in a specified IDO collection is marked as new.
object.IsObjectNew( integer )
Part |
Description |
| object | Required. The name of a valid IDO collection object. |
| integer | Required. The index number of an object in the entries for the current IDO collection. |
A return value of:
If the specified IDO collection might not have focus, use this method. If the specified IDO collection has focus, use the IsCurrentObjectNew method.
Sub Main()
Dim i As Integer
i = ThisForm.PrimaryIDOCollection.GetCurrentObjectIndex()
If ThisForm.PrimaryIDOCollection.IsObjectNew(i) Then
Application.ShowMessage("This is a new record.")
End If
End Sub