WinStudio

IsObjectNewAndUnmodified Method

Applies To

IWSIDOCollection interface

Definition

Returns a Boolean value indicating whether the object in a specified IDO collection is marked as new and has not been modified.

Syntax

object.IsObjectNewAndUnmodified( integer )

  Part

  Description

object Required. The name of a valid IDO collection object.
integer Required. The index number of an object in the entries for the current IDO collection.

Remarks

A return value of:

If the specified IDO collection might not have focus, use this method. If the specified IDO collection has focus, use the IsCurrentObjectNewAndUnmodified method.

Example

Sub Main()
    Dim i As Integer
    
    For i = 0  to ThisForm.PrimaryIDOCollection.GetNumEntries() - 1
        If ThisForm.PrimaryIDOCollection.IsObjectNewAndUnmodified(i) Then
            ThisForm.Components("PaymentTypeCombo").Text = ""
        End If
    Next i
End Sub