WinStudio
IWSForm interface
Returns a string containing the value returned to the parent form from the last modal child find form. Read-only.
object.LastModalChildFindResult
Part |
Description |
| object | Required. A reference to the parent form for the modal child find form. |
The return value is a string containing the result returned to the parent form from the modal child find form. The return string uses the ~LIT~(...) syntax to denote the result from the modal child form that was returned to the parent form.
An example of a modal child find form is the query form that is displayed when a user right-clicks in a component and selects the Find command. The user uses the modal child find form to issue a query and find a value for the component. If the user selects a value from the results of the query and clicks OK, then the selected value is returned to the component on the parent form.
Sub Main() Dim strFindResult As String strFindResult = ThisForm.LastModalChildFindResult Application.ShowMessage(strFindResult) End Sub