WinStudio
IWSFormComponent interface, list source objects
Inserts entries into the list for a list source object.
object.ListSourceScriptAddListItem( string )
Part |
Description |
| object | Required. The name of a valid component object. |
| string | Required. The name of the new tab-delimited list item. |
Typically, use this method in a script that functions as the list source for a component with a drop-down list (DropList component). However, you can also use it with List, ComboBox, or GridColumn components.
This API must be used from a global script that is referenced in the component's list source, where the list source is of type Script.
Sub Main() ThisForm.Components( "ListComboBox" ).ListSourceScriptAddListItem( "Item 1" ) ThisForm.Components( "ListComboBox" ).ListSourceScriptAddListItem( "Item 2" ) ThisForm.Components( "ListComboBox" ).ListSourceScriptAddListItem( "Item 3" ) ThisForm.Components( "ListComboBox" ).ListSourceScriptAddListItem( "Item 4" ) ThisForm.Components( "ListComboBox" ).ListSourceScriptAddListItem( "Item 5" ) End Sub