WinStudio
IWSIDOCollection interface
Determines whether the collection will be loaded in first-to-last order (False) or last-to-first order (True). The default is False.
object.LoadInReverse
Part |
Description |
| object | Required. A reference to an IDO collection object. |
object.LoadInReverse = Boolean
Part |
Description |
| object | Required. A reference to an IDO collection object. |
| Boolean | Required. A Boolean value indicating whether the collection will be retrieved in ascending (True) or descending (False) order. |
With the default behavior (this property set to False), using the initial Refresh action or exiting Filter-In-Place gets the top n rows, and the GetMoreRows method retrieves batches of n rows in descending order, appending them to the collection. If this property is set to True, the initial Refresh gets the last n rows, and the GetMoreRows method retrieves batches of n rows in ascending order, prepending them to the collection.
NOTE: When changing this setting, do not immediately call GetMoreRows. A call to Refresh or to leave Filter-In-Place should follow.
Sub Main() ' Loads the primary collection backwards If Not ThisForm.PrimaryIDOCollection.LoadInReverse Then ThisForm.PrimaryIDOCollection.LoadInReverse = True ThisForm.PrimaryIDOCollection.Refresh() End If End Sub