WinStudio
IWSIDOCollection interface
Sets the current object in the specified IDO collection to "modified" based on the specified criteria.
object.SetCurrentObjectModified( Boolean )
Part |
Description |
| object | Required. A reference to a valid IDO collection object. |
| Boolean | Required. Determines whether the object is marked
as "modified":
|
Sub Main()
If ThisForm.PrimaryIDOCollection.GetCurrentObjectProperty("SelectFlag") = "1" Then
ThisForm.PrimaryIDOCollection.SetCurrentObjectModified(False)
End If
End Sub