WinStudio
IWSIDOCollection interface
Sets the property of an object in a specified IDO collection to "modified", based on specified criteria.
object.SetObjectPropertyModified( string, integer, Boolean )
Part |
Description |
| object | Required. A reference to a valid IDO collection object. |
| string | Required. The name of the object property. |
| integer | Required. An integer indicating the index number of an object in the entries for the current IDO collection. |
| Boolean | Required. Determines whether the object property
is marked as "modified".
|
Sub Main() Dim i As Integer Dim SubColCache As IWSIDOCollection Dim strCompare As String SubColCache = ThisForm.Components(GetParameter(0)).IDOCollection For i = 0 To SubColCache.GetNumEntries - 1 If (SubColCache.IsObjectNew(i)) Then strCompare = SubColCache.GetObjectProperty(GetParameter(1), i) If (strCompare = GetParameter(2)) Then SubColCache.SetObjectForceUpdate(i, True) SubColCache.SetObjectNew(i, False) SubColCache.SetObjectPropertyModified(GetParameter(1), i, False) End If End If Next i End Sub