WinStudio
IWSApplication interface
Displays a string in a message box, waits for the user to click a button, and then returns an integer indicating which button the user clicked.
Application.ShowMessage( string [, style ] )
Part |
Description |
| string | Required. The "prompt" string, containing the text to be displayed as the message in the box. |
| style | Optional. Visual Basic MsgBoxStyle setting
that determines what buttons and icon are displayed in the message
box.
For more information, see the "Message Box Style Settings" section later in this topic. |
This method provides the same type of functionality as the MsgBox Function in Visual Basic. This method is designed to support various locale settings for international compatibility by reconciling the current system default locale with the font setting to display messages properly.
The prompt string (string1) can be a combination of literal and variable values, as in the following example:
("The
RGB code for your default form background color is " & defColor)
To concatenate string parts, use the ampersand (&) character.
This method does not support a Help button for context-sensitive help.
For more information, including button parameters and return values, see the online Help for the Visual Basic MsgBox Function.
The following table lists the message box style (MsgBoxStyle) options, how the system presents each, and the return values for each button.
| Option | Buttons | Description / Comments |
AbortRetryIgnore |
Abort Retry Ignore |
Equivalent to vbAbortRetryIgnore. |
ApplicationModal |
OK |
Equivalent to vbApplicationModal. |
Critical |
OK |
Equivalent to vbCritical. |
DefaultButton1 |
OK |
Equivalent to vbDefaultButton1. |
DefaultButton2 |
OK |
Equivalent to vbDefaultButton2. |
DefaultButton3 |
OK |
Equivalent to vbDefaultButton3. |
Exclamation |
OK |
Equivalent to vbExclamation. |
Information |
OK |
Equivalent to vbInformation. |
MsgBoxHelp |
OK |
Equivalent to vbMsgBoxHelp. |
MsgBoxRight |
OK |
Equivalent to vbMsgBoxRight. |
MsgBoxRtlReading |
OK |
Equivalent to vbMsgBoxRtlReading. |
MsgBoxSetForeground |
OK |
Equivalent to vbMsgBoxSetForeground. |
OkCancel |
OK Cancel |
|
OkOnly |
OK |
|
Question |
OK |
Equivalent to vbQuestion. |
RetryCancel |
Retry Cancel |
Equivalent to vbRetryCancel. |
SystemModal |
OK |
Equivalent to vbSystemModal. |
YesNo |
Yes No |
With this style, the close message box button is disabled. Equivalent to vbYesNo. |
YesNoCancel |
Yes No Cancel |
Equivalent to vbYesNoCancel. |
Sub MsgBox()
Dim defColor As String
defColor = Application.GetUserPreferenceValue("BaseFormBackColorDescriptor")
Application.ShowMessage("The RGB code for your default form background color is: " & defColor)
End Sub