WinStudio
IWSApplication interface
Opens a standard Windows Save File dialog box, optionally passing the path and name of a file to save; and returns the path and file name the user sets.
Application.ShowSaveFileDialog( string1, string2, string3, [ string4, string5 ] )
Part |
Description |
| string1 | Required. By reference, the path and name of the file to be saved. |
| string2 | Required. The text that appears in the title bar of the Save File dialog box. |
| string3 | Required. A string containing a pipe-delimited
list of file extension filters. These filters control what is
displayed in the file selection field.
These filters must each use the format:
Example: The following example causes the Files of type drop-down list in the Save File dialog box to include options for JPG, PNG, and All files.
To specify no filters, use an empty string ( |
| string4 | Optional. The extension that the system should
add as the default extension to a file name if no other extension
is specified.
For example, suppose you specify "txt" for this string. If a user then specifies MyFile as the file name (with no extension) then the system automatically appends a dot ( . ) and this default extension. In this case, the system returns the file name as MyFile.txt. If the user does specify an extension, (for example, MyFile.doc or MyFile.txt), then the system appends nothing to the file name. To specify no default extension, use an empty string ( If you use this parameter, you must also use string5, and vice versa. |
| string5 | Optional. The full path to the default folder to
open when the Save File dialog box opens.
Example: If the specified folder does not exist, the system defaults to whatever the "current" folder is. To specify no default path, use an empty string ( If you use this parameter, you must also use string4, and vice versa. |
The return is a string containing the path and file name under which the user saved the file.
Public Sub SaveFileDialog()
Dim FileName As String
FileName = String.Empty
Application.ShowSaveFileDialog(FileName, "Save File", _
"JPG files (*.jpg)|*.jpg|PNG files (*.png)|*.png|All files (*.*)|*.*", _
"", "C:\WINDOWS\Web\Wallpaper")
Application.ShowMessage("Test value = " & FileName)
End Sub