WinStudio

TreeSetNodeImageAt Method

Applies To

IWSFormComponent interface, tree objects

Definition

Sets the image for a specific node in the normal, unselected state to display.

Syntax

object.TreeSetNodeImageAt( string1, string2 )

  Part

  Description

object Required. A reference to a valid tree component object.
string1 Required. The tree node ID (GUID) or node index series.
string2 Required. The image file name.

Remarks

The image can be defined using an explicit file path; otherwise, WinStudio uses the current working directory to locate the image file.

For more information on the GUID and index series, see Notes on the Tree Node ID (GUID) and Index Series.

Examples

ThisForm.Components("graph1").TreeSetNodeImageAt("My Tree Node ID", "MyImage.jpg")
ThisForm.Components("graph1").TreeSetNodeImageAt("2,0", "MyImage.png")