WinStudio
IWSIDOCollection interface
Performs operations related to the current object in a collection that WinStudio normally performs after a save current operation (see "Remarks" below).
object.UpdateCurrentStatePostSave( )
Part |
Description |
object |
Required. A reference to a valid IDO collection object. |
This method is designed to be used in conjunction with the SaveCurrentDeferStateUpdate method. The operation of the two methods on the current object in a collection is similar to the operation of the UpdateStatesPostSave method and the SaveDeferStateUpdate method on all objects in a collection.
This method does not save the object and must be used with caution because data changes appear to have been committed to the database.
Sub Main() Dim bSuccess As Boolean Dim ReturnValue As String bSuccess = ThisForm.CurrentIDOCollection.SaveCurrentDeferStateUpdate() If (bSuccess) Then End If If (bSuccess) Then ThisForm.CurrentIDOCollection.UpdateCurrentStatePostSave() Else End If ReturnValue = "-1" End Sub
SaveCurrentDeferStateUpdate Method