WinStudio
Occurs before WinStudio creates a new object in a collection or subcollection, initializes it with values from the current object, and makes the new object the current object during execution of:
The default implementation of the StdFormCopy event
An event handler of the type Collection Copy
The Copy method in a script
The default implementation fires the following sequence of standard events:
StdObjectNew
StdObjectSelectCurrent
StdObjectSelectCurrentCompleted
StdObjectNewCompleted
Your application cannot call the default implementation by generating the event.
The default implementation is a collection-level operation, which can occur in a collection whether or not the collection is current.