WinStudio
Occurs before WinStudio navigates to the last object in a collection or subcollection during execution of
The default implementation of the StdFormLast event
An event handler of the type Collection Navigate for which the parameter Last is specified
The Last method in a script
The default implementation fires the following sequence of standard events:
StdObjectLast
StdObjectSelectCurrent
StdObjectSelectCurrentCompleted
StdObjectLastCompleted
Your application cannot call the default implementation by generating the event.
The default implementation is a collection-level operation, which can occur in a collection whether or not the collection is current.