WinStudio
Occurs before WinStudio retrieves the current object in the collection from the middle-tier IDO during execution of one of the following:
The default implementation of the StdFormRefreshCurrent event
An event handler of the type Collection Refresh Current
The RefreshCurrentObject method in a script
The default implementation fires the following sequence of standard events:
StdObjectRefreshCurrent
StdObjectRefreshCurrentCompleted
Your application cannot call the default implementation by generating the event.
The default implementation is a collection-level operation, which can occur in a collection whether or not the collection is current.