Reauthorizing a Credit Card upon Shipment

You can avoid reserving funds against the customer's card too early, but still ensure that the customer has the necessary funds before you ship the product. To do this, run a pre-authorization of 0 dollars (or whatever currency is being used) during order entry. Then use the Credit Card Shipping Authorization Utility to perform another authorization for the full amount of the order just before you ship the product.

Note: This utility is intended to be run after the order has shipped in SyteLine  but before the product is physically shipped from the building.

In the Credit Card Shipping Authorization utility:

  1. Specify criteria that the utility uses to select the transactions to process:

    Order

    Specify the starting and ending customer order numbers to reauthorize.

    Date Shipped

    Specify the date range of shipped orders to reauthorize.

    Ship Via

    Specify a shipping carrier, or a range of carriers, to limit the reauthorization only to orders handled by that carrier, or range of carriers. This is useful if you want to run the utility multiple times based on when a certain shipper is due to arrive each day.

  2. Select a report generation option:
  3. Click Process. The report output displays the credit card transaction details. The reference pointer to the third-party credit card processing application is displayed in place of the actual credit card number.

Notes


Related Topics

Pre-authorizing Credit Card Amounts or Percentages