This is the web address of the synchronous XML interface to this Intranet. It is used primarily by WinStudio clients which are configured to connect via the Internet. It may also be used by system integrators for programmatic access to a site on this intranet.
You must specify a fully qualified URL. It should be the address of the ConfigServer, which is deployed on your utility server when you include the web server feature of the utility server setup. For example, if the machine name is UTILSERVER, then the URL might look like this:
http://UTILSERVER/IDORequestService/ConfigServer.aspx
Or if you want to use secured http - a good idea if this server will be open to the internet for http traffic - use this format:
https://UTILSERVER/IDORequestService/ConfigServer.aspx
This field is active only if HTTP is selected in the Transport field.