Password Set Date

This field on the Users form indicates the date that the user password was last set. Normally, this field is set automatically to the current date whenever the password is changed. However, system administrators can manually reset this field if necessary.

One example of when this field might need to be set manually is if, for some reason, the user needs to reset the password but has recently changed it, within the time allowed by the Password Minimum Days field on the Password Parameters form. In a case like this, the system administrator can manually change the date in this field to a date earlier than the Password Minimum Days window. The password can then be changed, either by the user or the system administrator.