Persistent

On the Event Variable Groups form, when selected, this check box indicates that the variable's value is to be passed on to subsequent event handlers in the sequence, except those which refer to an initial state that contains the same variable, in which case that initial state's value is used for that handler.

When cleared, the variable's value is reset by each succeeding event handler that uses it.

NOTE: This option is available only for synchronous event handlers. This setting does, however, affect any asynchronous event handlers that intervene in the sequence.

On the Event Handler Status form, this field is display-only.


Related Topics

Event Variable Groups Forms

Event Handler Status Form