Event Actions

Use this form to create, view, modify, and delete event actions. Event actions are defined as units of work the system performs when an event is triggered and executes an event handler. Event handlers can include one or more actions as part of their definitions.

To create new event actions, you must open this form using the Event Actions button on the Event Handlers form. If you open this form from the Explorer or the Select Form dialog box, you can only view and modify existing actions. For the procedure to create an event action, see Creating Event Actions.

For guided assistance in setting parameters for an event action, click the Edit Parameters button. Advanced users can click the Show Details button to display tabs where you can manually enter the parameter information. Otherwise these tabs are hidden.

Use the Variable Access tab to limit the access that recipients of a message have to the designated variable value, and/or to set the caption for the designated variable. The variables you can limit in this manner must be variables that are used in sending event-related messages.

For information about application-specific workflow event handlers, see About Workflow Event Handlers.

For more information, see the following topics in the Guide to the Application Event System:


Related Topics

Events Overviews and Processes

Creating Event Actions

Event Handlers Form