Event Status
Use this form to:
	- View the status of events that are currently running.
 
	- View the history of events that have finished running.
 
	- Retry all retryable handlers and attempt to continue executing 
	 previously un-run handlers, if possible.
 
	- View the Voting status for outstanding Prompt actions.
 
This form has five tabs:
	- The Event tab provides options to filter for events and 
	 handlers in various states and make it easier to locate specific ones. 
	 For example, suppose you want to find data about all events that are 
	 currently suspended. With Filter-in-Place, select the Suspended check 
	 box, then execute Filter-in-Place.
 
	- The Handlers tab shows data about handlers that are currently 
	 processing or finished processing.
 
	- The Parameters tab shows data about the parameters associated 
	 with an event that is currently running. These include input parameters 
	 passed into the event, as well as output parameters created by handlers' 
	 actions.
 
	- The Output Parameters tab shows data about the output parameters 
	 of an event that has finished running.
 
	- The Voting tab shows information about the voting status 
	 of a Prompt.
 
For more information, see "Tracking Event System Status" in 
 the Guide to the Application Event System.
Related Topics
Events Overviews 
 and Processes
Event Handler 
 Status form
Event Handler 
 Revisions form