System Configuration Parameters

Use this form to view and set parameters that the event system uses in conjunction with the Framework Event Service for each system logon configuration. These parameters are used solely within the application event system.

You can have a different set of parameters for each logon configuration your system has.

The settings on this form override any corresponding settings on events-related forms when there is a conflict.

For example, if you set a minimum retry interval of 300 seconds on the Event Triggers form, and you have the Minimum Interval field on this form set to 600 seconds, the system waits 600 seconds between retries.

To define settings for a configuration, in the Configuration Name field, enter the name of the system configuration and then enter the appropriate values in the other fields. For details, see the Help for those fields.


Related Topics

Events Overviews and Processes

Event Triggers Form