IDO Properties

Use this form to view or define properties associated with an IDO.

On the Property Overrides tab, an asterisk (*) to the left of a field label indicates that the field value is defined for the property only and is not inherited from a property class. If a field contains a value and there is no asterisk next to the label, the value is inherited from a property class.

You cannot override a value inherited from a property class with a null value on the Property Overrides tab.

The Implementation tab is enabled only for properties where the Property Type is Derived or Unbound.

The Subcollection tab is enabled only for properties where the Property Type is Subcollection.


Related Topics

Understanding Properties

Adding a Property to an IDO

Editing an IDO Property

Deleting a Property from an IDO

Exporting and Importing Property Classes