Use the New IDO Wizard to define a new IDO and add it to a project.
This wizard is a multi-page form:
Page |
Use/Comments |
1 |
On this page, you must specify:
For more information about these and the other options available on this page, right-click the desired option and select Help. To move to page 2, click Next. NOTE: If you specify a value for the Extends attribute, page 2 of the wizard is not used and the Next button is disabled. In this case, click Finish. |
2 |
Use this page to:
By default, all of the columns in the primary base table are included as properties in the IDO. When you are finished, click Finish. |
Including Data from an Oracle Database into a Mongoose Application
Including Data from a Different SQL Database into a Mongoose Application