SyteLine comes with many predefined application messages that you can use as needed. If no predefined message is sufficient, use this form to create your own messages and add them to the ApplicationMessages table.
The ApplicationMessages table contains the translatable text to be used in messages that are initiated from within the application. Although multiple language versions of a message can be stored in the ApplicationMessages table, the Maintain Application Messages form works only with US English messages, that is, messages where the MessageLanguage is specified as "1033" or the Language ID as "en-US".
For information about how to use this form to create messages, see About Application Message Construction.
About Application Message Construction
Building Constraint Exception Messages
General Parameters form