PROPERTYAVAILABLE
Lets form and application developers know when an invalid reference
to a property has taken place or is about to take place. This allows developers
to develop in such a way that they can choose either:
- To bypass the property referenced by this function (by checking
before the property
is actually referenced), when an invalid return is indicated;
or
- To check whether an invalid value was returned from the
referenced property (by checking after
the value is returned).
Return Value
Boolean
A value of TRUE indicates that the property and/or its return value
is available. A value of FALSE indicates that the property and/or its
return value is not available.
Syntax
PROPERTYAVAILABLE( string propertyName
)
where propertyName is a reference
to a named property in one of these:
- P( ) or PROPERTY(
) function
- PROPERTYMODIFIED( )
function
- SETPROPVALUES( ) application
event system keyword
Used with Framework Events
- IdoOnItemInsert
- IdoPostItemInsert
- IdoOnItemUpdate
- IdoPostItemUpdate
- IdoOnItemDelete
- IdoPostItemDelete
- IdoOnLoadCollection
- IdoPostLoadCollection