Scheduling Background Tasks (Developer/Administrator)
The application runs reports as background tasks that are placed on 
 a "queue" to be run in order. You can also set up other tasks 
 to run in the background. The TaskMan Windows service polls the list of 
 Active Background Tasks and executes any new task that is posted to the 
 queue with a status of READY.
SQL Server Agent must be running on the database server in order to 
 perform background processing.
For more information about TaskMan, see the Infor SyteLine Administration Guide 
 or the Reporting 
 Guide.
Create a Background Task
	- Create a new record on the Background 
	 Task Definitions form.
 
	- Specify a task name (for example, RunCustomerOrderReport) and description.
 
	- Specify an executable: 
	
		- For a report, specify the name of the report (for example, 
		 CustomerOrder) in the Executable Name field and the type of executable 
		 (RPT) in the Executable Type field.
 
		- For a stored procedure, specify the procedure name in the Executable 
		 Name field and select SP in the Executable Type field.
 
		- For an executable program, specify the program name and path 
		 (for example, c:\Infor\myprog) in the Executable Name field and 
		 select EXE in the Executable Type field.
 
		- For an IDO method, specify the method name (in the format IDO.Method 
		 - for example, MyProgID.SLSites.MyTestMethod) in the Executable 
		 Name field and select IDOMTH in the Executable Type field.
 
	
 
	- Click the buttons on the form to specify any report options or 
	 excluded tasks.
 
	- Save the record.
 
Your new background task can be called from any form as an event handler.
Check to See if the Task is Running
When TaskMan starts a task, it updates the Started field in the Status 
 Information group box. If the Completed field is blank, the task is still 
 running.
Also, you can see which tasks are currently running by opening the Active 
 Background Tasks form.
View Details About the Completed Task
After TaskMan has completed the task, even if it fails, you can view 
 details about its execution on the Background 
 Task History form. Details include:
	- Task description
 
	- Return status
 
	- User who submitted the task
 
	- Messages triggered by the task
 
Returning Error Information from an Executable
To get information back to TaskMan from an executable, use any of these 
 methods in the EXE:
	- Put a message in the ProcessErrorLog table. These messages appear 
	 in the Task Messages tab on the Background Task History form.
 
	- Print the error message in a file called
	
	taskman-install-directory\Output\task-name_task-number.txt
	
	(for example, C:\Program Files\Infor\SyteLine\Output\APChecks_435.txt) 
	 TaskMan will use this as an error message in the Background Task History. 
	- Return an integer error code. TaskMan puts the EXE return code 
	 in the BGTaskHistory table, with return code 0 indicating success.
 
Related Topics
Modifying 
 Forms to Submit Tasks to the Background Queue