Synchronizing Forms Only

You can synchronize only the forms, without affecting global objects or the Explorer in the Target configuration.

When you use the form-only option, FormSync does this:

CAUTION: Before synchronization, make sure you back up the forms database in the Target configuration and confirm your database and server settings. For more information, see Before You Use FormSync.

To synchronize forms only:

  1. Open the Form Sync form, specify your Source and Targe configurations, and click OK.
  2. From the Synchronization base level drop-down list, specify whether you want to synchronize objects at the Vendor, Site, or Group level.

    For more information, see Synchronization base level.

  3. In the Log detail field, specify the level of detail you want to record in the log.

    For more information, see Log Detail Levels.

  4. Select the check box labeled Only process objects changed at the synchronization base level.
  5. On the Forms tab, select Merge customized forms with base-level forms.
  6. Click Merge Options.
  7. On the Merge Options page, do one of these actions:
  8. Click OK.
  9. (Optional) In the Form name field, specify one or more forms to synchronize.

    For more information, see Form name.

  10. (Optional) To remove all users' form run-time changes from the form, select the Remove runtime changes when form replaced option.

    For more information, see Understanding WinStudio Customizations.

  11. On the Explorer tab, clear the Update check box, and select the Keep customizations check box.
  12. On the Global Objects tab, select Keep customizations, and clear all check boxes in the Filter group box.

    To clear all the check boxes at once, use the Toggle All/None option at the end of the list.

  13. Click Synchronize.

Related Topics

About Synchronization