Use this dialog box to find a record that contains a specified value in a field.
If there is a match, the system displays the first record that contains a matching value. To find the next matching record, press CTRL+F2.
The sort order of the collection determines the order in which you find matching records. For more information about sort order, see Sorting Collections.
Note that this search applies only to a collection that has already been retrieved and does not query the database again. If you need to search all records, you can, if necessary change the cap on records retrieved. For more information, see Caps on Collections.
The following table lists the elements of this dialog box and explains their use.
| Element | Function/Comments |
|---|---|
| Find | Type the value you want to find, such as a word or number.
The Find feature uses what is known as an "implied wildcard" search. For more information, see Implied Wildcards. |
| In Collection | From the drop-down list, select the name of the collection
you want to search, if it is different from the one displayed.
If you do not know the name, return to the form and click About This Form on the Help menu to see the name of the current collection. |
| In Property | From the drop-down list, select the name of the field you want to search, if it is different from the one displayed. |
| Case Sensitive | To find records that have the exact capitalization you typed, select this check box. |
Finding a Value in a Collection of Records