Use this dialog box to replace values in a field with a new value that you specify.
The following table lists the elements of this dialog box and explains their use.
| Element | Function/Comments |
|---|---|
| Replace | Enter the value that you want to find and replace.
The Replace Value feature uses what is known as an "implied wildcard" search. For more information, see Implied Wildcards. |
| All Values | To replace the contents of a particular field in all records,
regardless of the field's current values, select this check
box.
To selectively replace the contents of a field only if it contains the value you entered in the Replace field, clear this check box. |
| With | Enter the value you want to replace the value you entered in the Replace field with. |
| In collection | From the drop-down list, select the name of the collection
you want to search.
If you do not know the name, return to the form and click About This Form on the Help menu to see the name of the current collection. |
| In property | From the drop-down list, select the name of the field you
want to search.
The default value for this field is whatever field the cursor was in when you opened this dialog box. So, to have the field in which you want to replace values preselected here, make sure that field is selected when you open this dialog box. |
| Case-sensitive | To find records that have the exact capitalization you
typed, select this check box.
For example, to find any value that contains the string "test", regardless of case, you might enter Test and clear this check box. This would locate values such as Test case, Amy's testing results, Sales Contest. If, however, you entered Test and selected this check box, the search would find only Test case from the previous list of results. |