Copying Selected Cells to a Spreadsheet
You can copy a single cell or a block of cells from a collection to
a spreadsheet.
These steps assume that you have the form open and showing the collection
you want to copy from.
NOTES:
- Row labels
are pasted in the spreadsheet as the first column. The labels
are for reference only and should not be copied and pasted back
into a grid. In the spreadsheet, you can delete the row-label
column, unless you want to keep it for reference purposes.
- Carriage returns and line feeds in a multi-line cell are removed
when you copy a row to the clipboard. So, if you have multi-line
cells, you must copy those cells separately or reconstruct them
in the spreadsheet.
To copy a single cell to a spreadsheet:
- Click in the cell you want to copy.
- Press CTRL+C, or select Edit > Copy. This action copies
the contents of the cell to the system clipboard.
- In your spreadsheet application, select the cell where you want
to copy the contents.
- Press CTRL+V or use the command your spreadsheet program uses to
paste in the material.
To copy a block of cells from a collection to a spreadsheet:
- Click in the first (upper-left) cell you want to copy.
- Shift-click in last (lower-right) cell you want to copy. The block
of cells is selected and highlighted.
You cannot select non-adjacent cells. That is, you can use CTRL-click
to select multiple non-adjacent cells, but when you paste them into
the spreadsheet only the first cell (or first contiguous block of
cells) actually gets pasted into the spreadsheet.
Alternatively, you can select the cells to copy by pressing shift-up,
shift-down, shift-right, and shift-left.
- Press CTRL+Insert. This action copies the selected block of cells
to the system clipboard.
- In your spreadsheet program, select the cell you want to be the
first (most upper-left) cell for the pasted columns.
- Press CTRL+V or use whatever command your spreadsheet program uses
to paste in the material.
Related Topics
Copying
Data To/From a Spreadsheet
Copying
Entire Collections to a Spreadsheet
Copying
Selected Columns to a Spreadsheet
Copying
Selected Records to a Spreadsheet
Pasting
Entire Collections into a Grid from a Spreadsheet
Pasting Selected
Records (Rows) from a Spreadsheet
Pasting
the Contents of a Single Cell from a Spreadsheet