With Automatic Resource Scheduling, appointments are automatically created for a service order during a cross-reference from an incident or during automatic service order generation.
You might want to automatically create appointments for resources in these cases:
Automatic resource scheduling creates appointments at the SRO header level. If your company schedules appointments at the line or operation level, this feature might not be beneficial.
To use this feature, you must turn on automatic scheduling of resources and then set some default values:
Scheduling Method
Specify the Scheduling Method to assign to the new appointment.
Appointment Status
Specify the status to assign to the new appointment
Hours
Specify the default hours to set on the new appointment if the amount cannot be acquired from other sources (see below).
In this form, you can also clear the Auto Dispatch SRO on Copy/Create option to override the default value set on the Service Parameters form, for the SRO being created here. This option is only available if the feature is enabled on the Service Parameters form.
The automatically created appointment is displayed in the grid section of the Schedules tab on the Service Orders form.
For SROs that are created from an incident or from Auto Generation, you can choose to automatically schedule appointments for the partner who is assigned to the task. To automatically assign a resource to the SRO, the system uses this hierarchy:
To determine the appointment hours and duration that are automatically assigned, the system uses this hierarchy:
The default values used for the automatic appointment are listed here:
| Appointment Field | Default Value |
| Reference | "SRO" |
| Reference Num | Number of the SRO |
| Appointment Status | Default from Service Parameters |
| Hours | See above |
| Method | Default from Service Parameters |
| Min Hours | Blank |
| Max Hours | Blank |
| Description | Description from SRO |
| Notes | Contents of first SRO note |