Material related to service work can be shipped to a different destination than the customer location associated to the service order. This provides flexibility for a technician to specify where they would like each part to be shipped.
Even though a customer or consumer has requested service, the material needed to fulfill the request may need to be shipped to a unique address. Use the Drop Ship Type and Drop Ship Number/Sequence with the SRO structure when using an alternative address.
The Drop Ship location for a Service Request Order (SRO) can be set at two levels:
You can store company address information in numerous areas of the system. Use the SRO Drop Shipment functionality to specify multiple location types:
Use the report options to specify the address you want to print on the paperwork. Choose from the customer of the order, the consumer, or the drop ship location.
Use the Service Order Packing Slip Generation utility to process and print packing slips by specific Drop Ship type and location. The Service Order Packing Slip Maintenance form shows the full address of the Drop Ship location when it exists. The Service Order Packing Slip report shows the appropriate shipment address, using a page break between different packing slip destinations.
The Drop Ship type and numbers are displayed in the SRO and Transaction areas of the Console when the Drop Ship Type has a value other than None.
The Drop Ship type and numbers have been added to set up service order templates specific to a drop ship destination.
For customers who use the Mobile Service solution and want to enable Drop Ship functionality, RSM UETs can be configured to store and pass these values.
Using SROs to Track Service Requests, Transactions, and Billing