Automating Updates to Unit Configurations

As service is performed on a unit, its configuration information may need to change to reflect the work that was done.  Use these areas of the system to automate the changes:

Material Transaction Posting

You can set up the system so that, when SRO Material Transactions are posted for service orders where a unit is specified on the SRO line, the unit's configuration can be changed accordingly. Use the Unit Configuration Update Method field on the Service Parameters form to handle this.

You can specify one of these options for the update method. For all options except Never, you must provide a reason code to use when a component is removed from the unit. By default, this method is set to Prompt.

When more than one serial-tracked item is issued, the system automatically creates multiple configuration records, one configuration for each serial number.

Notes:

Reversing a Material Transaction Posting

When the Configuration Update Method is set to Never, the system does not try to change the unit configuration when reversing a material transaction posting. For the other three options, the system tries to back out any changes to the configuration that were a result of the original posting.

SRO Material Data Collection

The data collection posting routine observes the unit configuration update method when set to Auto Synch or Auto Append. If the parameter is set to Prompt or Never, any posting on the form does not change the unit configuration.


Related Topics

Setting Up Service Parameters (SyteLine)