Copying Information from an Existing Unit

Use the Unit Copy modal form to copy the information from an existing unit to a new unit. Follow these steps to copy a unit:

  1. Click Create Configuration on the Unit Configuration form to launch the Unit Copy form.
  2. Specify this information:

    From

    Select the source from which you are copying the configuration.

    Job

    If the source is a job, select the job you are copying.

    Unit

    If the source is a unit, select the unit you are copying.

    Item

    If the source is an item, select the item you are copying.

    Install Date

    Specify the date of installation for the configuration. The current date is the default date.

    Create Units for Sub Components

    Select this check box to create sub components on the configuration. If cleared, only a configuration for the parent unit is created.

  3. Click Process to run the utility and complete the copy.

Related Topics

Using the Unit Configuration Form