Use the Service Appointment Status Codes form to maintain status codes used in service scheduling. Assign codes to schedule records to indicate the current status. Specify these fields on the form:
Appointment Status
Specify the identity of the appointment status code.
Closed
This field determines whether the appointment status code is an open or closed type. If the check box is selected and that status code is assigned to a schedule record, then it indicates to the user that the appointment has been completed.
Description
Specify a brief summary of what the appointment status code means.