Performing a Mass Creation of Partners

Use the Partner Create Utility to do a mass creation of partner records. Follow these steps to use the utility:

  1. For these fields, select the range to include:
  2. Select Include Customers to include the range of customers in the records.
  3. Select Include Vendors to include the range of vendors in the records.
  4. Select Include Employees to include the range of employees in the records.
  5. For each day, specify the maximum hours that a partner can be scheduled for a task or tasks.
  6. Specify this information:
  7. Select Override Employee Departments to use a department other than the one in which the partner works.
  8. Select Reimburse Material to reimburse the partner for material transactions on incidents that the partner is assigned. If this check box is cleared, costing is not affected for associated transactions.
  9. Select Reimburse Labor to reimburse the partner for labor transactions on incidents that the partner is assigned. If this field is cleared, costing for the associated transactions is not affected.
  10. Click Process to run the utility.

Related Topics

About Partners