Follow these steps to set up multi-day scheduling for a partner:
Source
Select the source of the work to be performed by the partner.
Partner
Select the partner for whom you want to set up the schedule.
Substitute
Specify the substitute partner to use if the assigned partner is not available.
Appointment Type
Select the type of appointment for the partner.
Appointment Status
Select the status of the appointment.
Appointment Start
Select the start date for the schedule.
Method
Select the method to use for assigning a partner to a task. Valid options are:
| Method | Description |
|---|---|
| Finite | Starting from the start date and time entered on the Multi-Day Scheduling form, the scheduling engine will schedule the partner for a certain number of days into the future. The engine will not schedule the partner for more hours than they are available to work. |
| Infinite | Starting from the start date and time entered on the Multi-Day Scheduling form, the scheduling engine will schedule the partner for a certain number of days into the future. The engine will schedule the partner for more hours than they are available to work. |
Hours
Specify the number of hours that a partner is to be scheduled for work on a particular task.
Minimum Hours Per Day
Specify the minimum amount of consecutive time that must be available before the task can be scheduled.
Maximum Hours Per Day
Specify the maximum amount of time to schedule in a day for the task.
Description
Specify a description of the work to be done.
In the Subject line, specify a subject for the note.
The Source Information group box shows this information derived from the source incident or SRO:
Click the Notes button to launch the modal Notes form.
Click View to view a linked form filtered for the selected source.
Scheduling Single Day Appointments