Use the Task Selection modal form to decide which tasks are displayed on the Scheduling board. Follow these steps to add tasks to the Scheduling board:
Select Tasks
Select this option to show only the tasks listed in the grid on the scheduling board when you click Apply To Display.
All Tasks
Select this option to show all scheduled tasks on the scheduling board when you click Apply To Display.
NOTE: All fields are disabled and filters are reset after selecting this option.
SRO Button
Click this button to launch the Select Additional Tasks modal form, which allows the user to manually add service orders.
Incident Button
Click this button to launch the Incidents form in filter mode and return the current incident upon closing the form.Additional Filters Button
Click this button to launch the Add Tasks modal form and add all incidents and SROs, down to the transaction level.
Add All Button
Click this button to add all incidents and SROs, down to the transaction level.Use the buttons on this form as described here:
Click MapPoint to launch MapPoint applications.