Setting Up Contract Line Entitlements and Surcharges

On the Service Contract Lines form, you can set up entitlements and surcharges for each contract line.

Entitlements

Specify the percentage amount that a customer is charged for each material or labor transaction. As service transactions are posted for the particular unit or item under contract, the system automatically calculates the price of the transaction based on the percentage not covered. For example, if labor is completely covered, then the % Of Coverage would be set to 100%. If only 10% of a transaction is going to be charged, then the % Of Coverage would be set to 90%. The system uses this formula:

The entitlement calculation can take into account different percentages based on the service order SRO Type, the Work Code of the labor transaction, or a combination of the two. For material transactions, the SRO Type and Family Code of the item determine the entitlement level.

You can create multiple labor and material coverage entries so that different work codes and family codes use a specific coverage value.

Surcharges

On the Contract Surcharges tab, specify surcharges for each contract line, allowing miscellaneous charges to be added to the contract. When invoiced, the contract pricing routine uses the percentage or fixed amount specified to calculate any surcharges. Charges can be recurring or one-time fees. You can set them up as a flat rate or a percentage of the contract price.

Surcharges are displayed as a line item on the contract invoice.


Related Topics

Using Contracts to Track Maintenance Agreements for Customers

Adding Contract Lines