Follow these steps to set up scheduling parameters:
Assign Lead Partner
Select this check box to assign the partner dispatched on an appointment as the lead partner of the SRO.
Dispatch Event Code
Select the code to use with an event when an appointment is linked to an incident.
Partner Start Address
Select the address to help MapPoint determine the starting point when plotting a route.
Partner End Address
Select the address to help MapPoint determine the ending point when plotting a route.
Default Scheduling Method
Select the method to use when entering a new appointment: Single-Day or Multi-Day. For more information, see Scheduling Method.
Display for Partner
Select the method to use to display Partner Information.
Header Date Format
Select the format to use to display the date when the view mode is set to Partner/Days, Work Week, or Partner Day/Time. For details regarding the syntax for a custom format, see Setting the Header Date Forms.
In the Dispatch Order section, specify the order of selection using the Field Order column and Required check boxes. You can mark each field as required if blank values are excluded.
Email Type
Select the type of email to use.
Email Server
Specify the server to use with the email.
Email Template
Specify a template to use for the email.
Use the pound symbol (#) before and after the field property name to substitute values from the screen. Follow this example for the email template:
Partner ID: #ParnterID# (#PartnerName#)