Setting Up Work Codes

Work codes represent the type of work that is recorded to a Service Request Order.

On the Work Codes form, specify this information about each type of work:

  1. Specify this information:

    Work Code

    Specify a unique alphanumeric code to represent the type of work that is recorded to a SRO.

    Description

    Specify an explanation for the type of work represented by the code. This description is used by default when selecting a work code on a form that also has a Description field.

  2. Specify this information:

    Cost

    Specify an hourly expense to associate with the type of work.

    Rate

    Specify an hourly charge to associate with the type of work.

  3. Specify these codes:

    Cost Code

    Select a cost code. Cost codes are used to classify project costs into categories. A cost code belongs to one of three cost classes:

    Cost codes are assigned to project transactions. These codes control which General Ledger accounts receive the transaction cost amount.

    Cost Code Description

    A description of the cost code is displayed.

    Tax Code

    Select a tax code, which represents how the sales tax is calculated. Selections are set up and maintained on the Tax Codes form.

    Tax Code Description

    A description of the tax code is displayed.

  4. Specify the Duration of time for the type of work.

Related Topics

Using SROs to Track Service Requests, Transactions, and Billing