Using Amortizations
An amortization is the reduction of the value of an asset by prorating
its cost over a period of time. Use amortizations to extend expenses over
a predefined period of time. Expenses such as contract maintenance for
a building, insurance payments or capital expenditures are examples of
occasions to create amortization schedules. You can create amortization
schedules to recognize revenue over a predefined period of time. You can
set up schedules manually and automatically.
Follow these steps to set up amortizations:
- Set the default options on the Service
Parameters form. Follow the steps in Setting
Up Amortizations.
- Create a new contract with annual Billing Frequency and fixed Billing
Type. Follow the steps in Adding a
Contract.
- Follow the steps in Adding
Contract Lines to add a contract line.
- Invoice the contract. Follow the steps in Invoicing
a Contract. The amortization is automatically created during contract
invoicing.
- The system debits the sales account from the distribution account
specified on the contract, and credits the amortization prepaid expense
account specified on the Service Parameters form.
- Use the Amortization
Transaction by Account Report and Outstanding
Amortization by Account Report to review details about amortizations.
Related Topics
About SyteLine Service
Setting Up Amortizations
Maintaining Amortizations
Scheduling Amortizations