The Chinese Book Definition form is used to define the Chinese account book and the six report layouts.
To generate the report:
A Three-Bucket report is only against 1 account and lists all of its transactions in a special period. It is a report with 3 numeric columns. For example, if there are 50 transactions in this period, then the report will have 50 lines of transactions and 3 columns.
A Multi-Bucket report is against more than one account, with each account information displayed in each column. For example, if five accounts are defined in the Multi-Bucket report, then five columns will be displayed. An unlimited number of columns (accounts) can be defined in this type of report.
The Book of Account report is similar to the Three-Bucket report, but it has a column for corresponding accounts. If there is more than one corresponding account, multiple lines show on the report.
This report is the foreign currency report for a Three-Bucket report.
This report is the foreign currency report for the Book of Account report.
The Tax-Bucket report is used for reporting taxes, such as VAT on accounts.