Click this button to calculate the tax on the selected order or estimate. This button is enabled only when you are licensed for the Tax Interface.
If the Calculate Order Entry Tax option on the Tax Interface Parameters form is selected, taxes are automatically calculated during order entry and wherever the system normally calculates tax on orders. Generally, that option should be selected; however, if you are having performance issues due to the number of times that SyteLine calculates sales tax on an order, you can turn off that option. You can manually calculate taxes at any time with this Calculate Tax button.
Invoicing always automatically calculates tax, as does the Order Verification Report.