Generate Ship Notice

Select this field to automatically generate advanced shipping notices (ASNs) by printing the bill of lading for this customer. ASNs are created during the printing of the bill of lading.

Clear this field if ASNs should not be created or if the bill of lading is not printed.

NOTE:A Customer Profile for ship to 0 must exist for the system to export ASNs. Also, ASNs are used during posting of 830/862s to SyteLine to determine net requirements for imported releases. If 830/862s are being processed and this option is cleared, ALL shipments from SyteLine orders must be manually recorded in the translator before exporting data from the translator.