Supplementary Statistical Declaration Value

Enter the Supplementary Statistical Declaration (SSD) Value, which is used in some European Union (EU) reports. The SSD value is the export value from the transaction, if it is specified. The value is the unit cost/price (not the extended cost/price) and is in the currency of the customer order or purchase order.

You can enter an SSD value on:

To update the SSD value, specify a non-zero value. After changing the value, if you want to reset it to the default, enter a value of zero and the system will follow the steps described above.

NOTE: The Foreign Value is the SSD value.