Use the Billing Terms form to identify and maintain billing terms to be applied to customers. The Billing Terms code displays on the Customers and Vendors forms (and their multi-site equivalents). You can identify default billing terms for each customer or vendor. The Billing Terms (sometimes called the Terms Code) determine the following:
For each customer or vendor, you can enter a Billing Terms code to use as a default when entering invoices. You must set up each code in the Billing Terms form before you can apply it to a customer or vendor.
NOTE: The system displays an error message if you attempt to delete a Terms Code currently being used in one of the following areas:
You can also create terms codes to use multiple due dates to allow the customer to pay a percentage of their invoice in installments.
NOTE: Multiple due dates for billing terms are not supported when running the Infor SyteLine Enterprise Financials Interface that works with Infor SunSystems.
You cannot use multiple due dates where you have either no Due Days or you have Discount Days.
System-generated debit memos should have multiple due dates if the terms code being used is a multiple due date terms code. This applies to debit memos generated via the following forms:
Setting multiple due dates in a terms code includes determining the following options:
Refer to the topic About Multiple Due Dates for Invoices and Debit Memos for further information about how multiple invoice due dates are used with invoicing and payments.
This chart example compares different combinations of Due Days, Cutoff Days, Prox Codes, Prox Due Days, Prox Months Forward, Prox Discount Days, Prox Discount Months Forward and Holiday Offset Method in order to determine the Due Date and Discount Date. 11/24/2011 is a holiday for these examples.
Invoice Date |
Prox Code/Due Days/Prox Due Day/Prox Months Fwd. |
Cutoff Day |
Holiday Offset Method |
Discount Days |
Prox Discount Day |
Prox Disc. Months Fwd. |
Due Date |
Discount Date |
Note (See Note Legend after this table) |
| 10/25/2011 | 0/30/0/0 | 25 |
No Offset |
10 |
0 |
0 |
11/24/2011 | 11/4/2011 | A |
| 10/25/2011 | 1/30/0/0 | 25 |
No Offset |
10 |
0 |
0 |
12/1/2011 | 11/4/2011 | B |
| 10/25/2011 | 2/30/0/0 | 25 |
No Offset |
10 |
0 |
0 |
11/30/2011 | 11/4/2011 | C |
| 10/25/2011 | 3/30/0/0 | 25 |
No Offset |
10 |
0 |
0 |
12/30/2011 | 11/4/2011 | D |
| 10/25/2011 | 99/30/0/0 | 25 |
No Offset |
10 |
0 |
0 |
11/24/2011 | 11/4/2011 | E |
| 10/25/2011 | 0/0/5/0 | 25 |
Bring Fwd. |
0 |
27 |
0 |
11/5/2011 | 10/27/2011 | F |
| 10/25/2011 | 1/0/5/0 | 25 |
Bring Fwd. |
0 |
27 |
0 |
11/5/2011 | 10/27/2011 | G |
| 10/25/2011 | 2/0/5/0 | 25 |
Bring Fwd. |
0 |
27 |
0 |
11/5/2011 | 10/27/2011 | H |
| 10/25/2011 | 3/0/5/0 | 25 |
Bring Fwd. |
0 |
27 |
0 |
12/5/2011 | 10/27/2011 | I |
| 10/25/2011 | 99/0/5/0 | 25 |
Bring Fwd. |
0 |
27 |
0 |
11/5/2011 | 10/27/2011 | J |
| 10/25/2011 | 0/0/24/0 | 30 |
Bring Fwd. |
0 |
10 |
0 |
11/23/2011 | 11/10/2011 | K |
| 10/25/2011 | 1/0/24/0 | 30 |
Postpone |
0 |
10 |
0 |
11/25/2011 | 11/10/2011 | L |
| 10/25/2011 | 2/0/24/0 | 30 |
No Offset |
0 |
10 |
0 |
11/24/2011 | 11/10/2011 | M |
| 10/25/2011 | 3/0/24/0 | 30 |
No Offset |
0 |
10 |
0 |
11/24/2011 | 11/10/2011 | N |
| 10/25/2011 | 99/0/24/0 | 30 |
No Offset |
0 |
10 |
0 |
11/24/2011 | 11/10/2011 | O |
| 10/25/2011 | 0/0/5/1 | 25 |
No Offset |
0 |
27 |
0 |
12/5/2011 | 10/27/2011 | P |
| 10/25/2011 | 1/0/5/1 | 25 |
No Offset |
0 |
27 |
1 |
12/5/2011 | 11/27/2011 | Q |
| 10/25/2011 | 2/0/5/1 | 25 |
No Offset |
0 |
27 |
0 |
12/5/2011 | 10/27/2011 | R |
| 10/25/2011 | 3/0/5/1 | 25 |
No Offset |
0 |
27 |
0 |
1/5/2012 | 10/27/2011 | S |
| 10/25/2011 | 99/0/5/1 | 25 |
No Offset |
0 |
27 |
0 |
12/5/2011 | 10/27/2011 | T |
A - Add Due Days to Invoice Date
B - Invoice Date >= Cutoff, Due Date is Start of Next Month plus Due Days
C - Due Date is End of Invoice Month plus Due Days
D - Invoice Date >= Cutoff, Due Date is End of Next Month plus Due Days
E - Add Due Days to Invoice Date
F - Invoice Day falls on or after Cutoff Day, move to next month
G - Invoice Day falls on or after Cutoff Day, move to next month
H - Invoice Day falls on or after Cutoff Day, move to next month
I - Invoice Day falls on or after Cutoff Day, move to next month, and then push to end of next month before adjusting to Prox Due Day
J - Invoice Day falls on or after Cutoff Day, move to next month
K - Holiday falls on 11/24/2011, Holiday Offset Method is Bring Forward
L - Holiday falls on 11/24/2011, Holiday Offset Method is Postpone
M - Holiday falls on 11/24/2011, Holiday Offset Method is No Offset
N - Holiday falls on 11/24/2011, Holiday Offset Method is No Offset
O - Holiday falls on 11/24/2011, Holiday Offset Method is No Offset
P - Prox Month to Forward is 1
Q - Prox Months Forward is 1; Prox Discount Months Forward is 1
R - Prox Month to Forward is 1
S - Prox Month to Forward is 1
T - Prox Month to Forward is 1