Customer Service Home - Tasks Tab
The Tasks tab contains three sections:
- Alerts - The buttons in this
section have red numbers if the number is above zero. The number is
green if it is zero. If you click the Past Due Lines button,
the Customer Order Lines form opens. If the number on the button
is red, the Customer Order Lines form displays the lines (the
red number on the button) that have a CO status and CO line status
of 'ordered', and the quantity shipped is less than the quantity ordered.
If you click the Past Due Releases button, that opens the Customer
Order Blanket Releases form. If the number on the button is red,
the Customer Order Blanket Releases form displays the number
of blanket CO releases that are past due as of today that have a CO
status and CO line status of 'ordered', and the quantity shipped is
less than the quantity ordered. If you click the Estimates to Expire
button, that opens the Estimates form. If the number on the
button is red, the Estimates form displays the number of estimates
that are about to expire within the next seven days that have estimate
and estimate line statuses of 'planned', 'quoted', or 'working'.
- Tasks - The tasks section lists
the tasks assigned to the logged-in user. See Adding
and Viewing User Tasks for more information about tasks.
- Inbox - The Inbox section lists
the messages for the logged-in user. See the Inbox
form for more information about the inbox. Double-click a field in
the Inbox grid to view all emails that share that value. All Inbox
fields can be filtered with the exception of Read and Expired.
EXAMPLE: To view only the emails
from John Doe, double-click John Doe in the From field.